This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24161B的BATGD的功能

Other Parts Discussed in Thread: BQ24161B, BQ24161

想用BQ24161B,但是芯片手册中没有BATGD这个管脚的定义,这个管脚应该如何接线呀。看名字,象是接到电池的负端。
  

  • 从PDF文档来看,跟24160的INT功能是一样的吧?从技术规格书的第5页来看,第7脚功能描述也是INT的功能,至于这个BATGD难道是BATGOOD?技术规格书第35页的图上,BQ24161的典型应用里,也是画的INT,而不是BATGD,是不是也代表这两个功能一致?

  • Datasheet的page 25有对于这个pin脚的详细描述

    9.3.18 Good Battery Monitor  The bq2416xx contains a good battery monitor circuit that places the bq2416xx into high-z mode if the battery
    voltage is above the BATGD threshold while in DEFAULT mode. This function is used to enable compliance to
    the battery charging standard that prevents charging from an un-enumerated USB host while the battery is above
    the good battery threshold. If the bq2416xx is in HOST mode, it is assumed that USB host has been enumerated
    and the good battery circuit has no effect on charging.

  • 这个pin脚用来检测电池的电压是否大于其判定门限,在default模式,使用BQ24161系列芯片,输入源需要兼容USB作为输入源时才采用。

    USB在100ms延迟后枚举所连接的负载的类型,如果没有经过枚举,将BQ24161B置于高阻状态以避免错误的枚举判断。

  • 谢谢,这个脚该怎么连线呢。

  • 楼主上电测量一下这个脚的电压,看看是否为3.8V左右(插入电池,插上适配器)。

    若是,悬空或者用个非常小的电容接到地.