This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25088MOS推动电压不足

您好!如图:希望做一个16-33V输入12v 5a输出的电源。空载或者带几百毫安载荷,都只有不到5v输出。

测量得:C1:17V  ;en脚2点几V,  C4:7.69v,C3:5.6v左右。由于示波器坏了。用万用表的最大最小值档位测量Q1的GS之间电压最大值不超过1V.  R4两端无明显电压,FB脚到地低于1V。Q1的s点一直跟电源输出电压一致。但取下Q1时,上电Q1的GS对应的焊盘上有8v左右的电压,但按上Q1就几乎没有电压了。换了几个板子结果一样。焊接上电阻我都量过应该没得问题。

请问这个是什么问题,如何处理。谢谢您。我的邮箱:sjdcz@163.com

桌面.zip