This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54620: 电源输出异常问题

Part Number: TPS54620


使用TPS54620芯片将5V转1V为FPGA供电,板子前期正常。前一段时间,板子正常运行一段时间后突然无1V输出,测量发现EN管脚为0V,VSENSE管脚也为0V,但PWRGD管脚为3.5V。

后续将芯片从板子上卸下,换到另一块全新的电路板上,仅焊接电源电路,测试发现VSENSE的输出为1.8V,最后分压得到的输出电压为2.5V左右,PWRGD管脚为0V。

请问有可能是什么原因使VSENSE不准?输出为0V时PWRGD管脚为何有电压?

最后附上电源设计电路