电路设计和datasheet基本一样,但是不能充电,不接电池时pack+电压为0.76V,感觉芯片在工作,可能是那里不对使它保护了,所以没有充电电压。我在R16上并一个0.1欧的电阻,pack+电压有16.3V,在我们的系统上是正常的,但是接上电池后再拔掉电池,pack+就又变成0.76V,不知道为什么,求指教,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路设计和datasheet基本一样,但是不能充电,不接电池时pack+电压为0.76V,感觉芯片在工作,可能是那里不对使它保护了,所以没有充电电压。我在R16上并一个0.1欧的电阻,pack+电压有16.3V,在我们的系统上是正常的,但是接上电池后再拔掉电池,pack+就又变成0.76V,不知道为什么,求指教,谢谢
电池插入的具体波形 在带有该功能的充电器芯片里都会给出,参考datasheet 中 Battery insert detection部分的检测波形示意图。以上谢谢!
波形我测过,datasheet反复看了几遍,现在的情况是输出没有波形,输出电压为0.76V
另外,将TS电压强行设置为1.55V后,有输出,但是波形不正常,电压也很高,有30V
请问有没可能是接地的问题,我把这部分电路的所有地都接的模拟地
温度检测脚,如果你给了9.31K欧姆和430K欧姆的偏置电阻,但实际的电路没有接NTC,那么芯片会认为是所接的NTC阻抗无穷大,触发温度保护。所以如果你没有接NTC,请用个10K的电阻替代它,即与430K欧姆电阻并联。
GND方面主要是注意隔离模拟地 和功率地。前面引脚配置的地与后端的开关电路的地隔离开来,在thermal pad实现单点接地。
7. Route the analog ground separately from the power ground and use a single ground connection to tie the
charger power ground to the charger analog ground. Just beneath the IC, use the copper-pour for analog
ground, but avoid power pins to reduce inductive and capacitive noise coupling. Connect analog ground to
GND. Connect analog ground and power ground together using the thermal pad as the single ground
connection point. Or use a 0-Ω resistor to tie analog ground to power ground (thermal pad should tie to
analog ground in this case). A star connection under the thermal pad is highly recommended
在没有插入电池时,会在pack+端检测到电池插入检测波形,即page 24的周期性的脉冲波形。以上谢谢!