This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560: TPS54560如何修改输出-15V时,如何EN引脚外部配置电路可以MUC的3.3V控制,符合芯片要求的电压范围?

Part Number: TPS54560


从官方的slva317b文档中查询到此电路,但缺少EN的外围电路,我需要24V输出输出-15V,EN接MUC的IO控制,0V输出关闭电源,3.3V高电平输出开启电源输出。

后续我查询《Working With Inverting Buck-Boost Converters》文档中有推荐的方法,但具体的MOS是P还是N没有具体说明,需要解答给出具体什么型号的MOS管?或者可行的具体电路?非常感谢了