This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM5013-Q1 was used to generated 12V DC power supply.
It looks to be working well when the input above 12.30V.
However, when the input decreased to 12.20V, it seems to be stopped, fre is almost 100Hz, which resulting in the output decreasing sharply.
The Minimum value is down to 6V and it results in The back-end cannot working. What can I do to advoid this case on the premise of not modifying the expected output.
Thank you for contacting TI China E2E forum and choosing our products as part of your solution.
Regarding your query, TI power design tool webench supports LM5013-Q1,
you can use this tool to review your design if there's anything issue with your circuit.
LM5013-Q1 data sheet, product information and support | TI.com