This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

24V铅酸电池芯片选型问题,急

Other Parts Discussed in Thread: BQ24450

输入为DC 36V, 给两节串联的额定12V铅酸电池充电,过充电压为29.6V,浮充电压27.6V,充电电流2.5A。想知道选BQ24450还是UC3909或者其他的芯片更合适?

另外,想问下预充电转恒流的电压为多少伏比较合适?预充电电流多大比较合适?

  • 亲;BQ24450比较合适。至于充电电流电压,建议咨询厂家。12V电池有免维护和阀控电池等多个种类,不同电池种类的值有些差异。

  • 2909属于比较早的控制芯片了,控制逻辑比较复杂,可以考虑选用BQ24450。

  • 想再问下,用BQ24450的话,当充电电流大于1A时,规格书上推荐使用的是PNP+NPN的准达林顿管,但是这样的达林顿管不好找,可以用PNP+PNP的达林顿管替代吗?或者用功率型的PNP管和NPN管组合一下?有合适的管子推荐吗?有用过24450的朋友能不能介绍下这个问题你们怎么解决的。