This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62736 Vin_OK指示无效



电路图是这样的,设置成3V输出,输出没有问题,但是无论输入从3.0V-4.2V怎么变化,Vin_OK脚一直是低电平,输入正常指示一直没有调出来,不知道是哪方面问题?我该从哪里修改?

  • 亲;貌似没啥问题,你感觉哪不对劲?

  • 这个问题我也发现了,你这组取样电阻值,VIN_OK的门限为3.3V左右,把VIN逐渐网上调,调到4.5V以上,VIN_OK是能输出高电平的,然后VIN往下调,VIN_OK一直能保持高电平知道VIN调到3.3V以下。这个和文档描述不符。

    要使VIN_OK在VIN为3.3V以上直接输出高电平,需要把R4/R5/R6这组的值放大,比如全部放大10倍以上,使得R4+R5+R6尽量接近13M,可以解决这个问题。

    不知道这是芯片设计问题还是文档没有讲到。