This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于电平转换的问题

Other Parts Discussed in Thread: TL431

我有一个关于电平转换的问题恳请大家能提供一些建议: 当我的系统输入为36~120V的时候,我将36~120V转化3.3V,然后送给DSP的GPIO口作为高电平,当我的系统输入为0V的时候,我将0V转化0V,然后送给DSP的GPIO口作为低电平。我目前想到的简单低成本设计是用TL431(因为TL431输出的2.499V能被DSP识别为高电平),如图:
                           
但是我发现TL431的Vka值最大为37V.....
请问这样使用的话会不会损害TL431,如果这种方式不可以,那么是否有其他的简单方法实现这种电平转换?