Other Parts Discussed in Thread: TPS54040
最近做的电路里,是输入12V,输出3.3V,输出电流150ma的,要求低功耗。想选择一个电源芯片,请帮忙推荐个型号。
还有选的芯片是开关的好还是ldo的好?有什么区别吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS54040
最近做的电路里,是输入12V,输出3.3V,输出电流150ma的,要求低功耗。想选择一个电源芯片,请帮忙推荐个型号。
还有选的芯片是开关的好还是ldo的好?有什么区别吗?
如果是选用LDO的,可以选TLV70433.
如果是开关形的,可以选TPS54040.
根据你的要求是低功耗,可以选用LDO的。但输入12V,输出3V,这样LDO的效率比较低。而DC/DC型,以TPS54040O为例,在输出为150mA下,其效率达90%。
LDO与DC/DC型的区别:
LDO:低压差线性稳压器的突出优点是具有最低的成本,最低的噪声和最低的静态电流。当系统中输入电压和输出电压相差比较大时,不能达到很高的效率。
DC/DC:其优点是效率高,输入电压范围较宽;其缺点是负载响应比LDO差,输出纹波比LDO大。