This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28750: 反激电源设计

Part Number: UCC28750

请教下,我最近在用UCC28750做反激设计,

DC400-700V,输出12V/1.2A,

按照fsw=65KHz,设计出来初级感量2.6mH,Dmax=0.2

问题1:变压器厂商反应初级感量过大,变压器体积很大

问题2:最大占空比才0.2,会出现管子的应力压力大、效率低等问题,可靠性是否存在较大问题

我的控制芯片选型是否存在问题,或者该工况不适合单端反激拓扑的使用

英文的E2E网站,似乎存在问题,无法提问