This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481升压问题



输入:3.6V~6V 输出12V 在输入为5V是输出为12V、1A,电流在负载变化的情况下为0~1A

现在输入3.6V时不能输出12V、在5V输入时负载较大时能够稳定输出12V,但负载变小就不行了,电流是一直达不到1A

我们是用万用板焊接的电路