This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于bq24133的简单疑问

Other Parts Discussed in Thread: BQ24133

想请问一下ti的工程师,最近我们想要选择一款锂电池充电ic,看了一下bq24133的datasheet ,觉得挺合适,但是有以下两点没太搞明白,希望解答:

1、如果开始由适配器对负载电路供电,如果突然拔掉适配器,此时将转为电池对负载供电,想确认一下,在切换过程中是否会造成负载瞬时断电?

2、同样上面的过程,如果换成电池先为负载供电,然后插上适配器,将转为适配器为负载供电,在由电池向适配器的切换过程中是否会造成负载瞬时断电?

(由于尚未细致阅读datasheet,问题如有不妥之处,你过来打我啊?)

  • 切换的过程不会造成系统负载的瞬间掉电,一个原因是切换的时间非常短,二是BQ24133有输出电容储能,负载有输入电容储能 可以平滑的过渡。

  • 典型的情况 请参考Figure 7. BATFET to ACFET Transition During Power Up ,可以看到从BAT切换到Adapter的过程是非常安全的。

  • 您好,我又有个问题想请教您一下,bq24133数据手册17页,底下一段话:

    Pull the TTC pin to AGND to disable both termination and fast charge safety timer (reset timer). Pull the TTC pin
    to VREF to disable the safety timer, but allow charge termination.

    文中说如果我将TTC接地,那么终止和快速充电计时器都disable,请问我应该如何理解这句话?

    是否意味着如果TTC接地了,那么电池充满电也不会停止充电,或者说此段中的充电终止只是特定情况下的充电终止?

  • 如果负载的电流和充电电流混合在一起 就不能进行正常的充电截止,而且由于负载电流会被当做充电电流,最大充电时间计数器会溢出。