Part Number: TPS546D24S
你好,能否提供并机堆叠4个的原理图?输入12V,输出2V/160A.是否可以5V/160A?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您对TI产品的关注!
关于你的咨询,你查询了我们的参考设计资源,没有这种低压差大电流输出的参考设计资源。
www.ti.com/.../index.html
我又查了下有关的资料。
我们评估板是2个堆叠的80A的,
堆叠4个180A可能也能达到,最好你那边测试评估下。
具体电路你可以结合2个堆叠的修改成4个的。Page7~Page9 schematic.