This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教TPS65150的一些细节

Other Parts Discussed in Thread: TPS65150

看了一下TPS65150的手册,感觉不是很详细,有一下一些疑问,还望TI帮忙解答:

1、电荷泵的FLYING电容与带负载能力的大概对应关系,另外是否可以选择0603的贴片电容

2、国产的SS14/24/34等肖特基二极管结电容比较大(100pF左右),是否可以满足电路中5个二极管的要求

3、GD是不是TI系列电源芯片的GOOD信号(手册上写的是Gate Driver,但是看原理框图又不像是用来外扩开关管的)?

4、VCOM Buffer与电位器分压相比,区别是什么?对于AT070TN92这种常规的液晶,是否需要使用VCOM Buffer功能?