This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100 電流滿刻度問題

Other Parts Discussed in Thread: BQ34Z100

各位大大好,想請問一些問題

1.目前採用BQ34Z100做電池的SOC/SOH的量測上的開發,預計放電電流達100A,而Datasheet中的資料"VA3 Input voltage range (SRP, SRN)為 Min:Vss-0.125 Max:+0.125",是否可藉由調整shunt resistance來提高到連量測達100A呢?(精度佔不考慮),因為目前採用40A去做電流校正,但實際操作上大於32A or -32A就為最大值無法再顯示在顯示更大的值,這有辦法處理到1:1的顯示?

2.若將100A-->至電流校正時填寫校正值為32A,但有選擇Chemistry而IC並不知道電流為(3.125:1)的狀態,則SOC與SOH的計算上??會精確嗎?如何得到正確的SOC與SOH。


  • 1. shunt阻值是一定要调整的,要是正常或者短路工作的两端的压差不超过125mV。

    2. 受到电量计内部寄存器长度的限制,16bit,最大显示+/-32768mA。 因此在校准的时候进行等比例的缩小,是可行的,相应的容量mAh的值也是要同比例的缩小。
    但是SOC 和 SOH 由于都是同比例的缩小,因此百分比不会受影响,依然可以显示正确的电量百分比。