This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217C启动时LDO1工作不正常

Other Parts Discussed in Thread: AM3352

PMIC:TPS65217C

CPU:AM3352 (ZCE封装)

参考设计:TI SLVU551I (Powering the AM335x with the TPS65217x)文档第8页图

问题描述:

我的设计和参考相同,LDO1带三个负载,VDDS, VIO, VRTC。但是AC的5V一上来,SYS(LDO1的输入)只能跟随保持几十ms就从5V掉到2.14V,LDO1的输出为零。

如果断开LDO1的三个负载,或者只接VDDS,则无问题,SYS的5V和LDO1输出的1.8V波形良好。基本可排除负载短路(三负载对地阻抗均80Kohm左右),请各位专家帮忙分析下还可能是什么原因?

我个人想法:

1. SLVU551I中介绍65217C应配合ZCZ封装的CPU使用,我的是ZCE,且文档第一页曰:This version does not support AM335x RTC-only operation。但此处应该无关紧要?

2. 怀疑有过流。看文档,65217还没active时,LDO1只支持1mA,但实际测量过每路负载的电流(断开其余两路),VDDS有个近40mA的上电电流,也没让LDO挂掉,反而是量不到电流的VIO会把LDO搞挂掉,这也是个让人疑惑的地方。

欢迎各位参与讨论,先行谢过。