TPS61175的规格书写的电流3A是只输出电流为3A还是只内部集成的MOS管的ID电流为3A,如果我需要用5V输入,24V/3A的输出用这颗IC合适吗?或者有更好的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
3A是开关限制电流:ILIM: N-Channel MOSFET current limit 3A(Min)~3.8A(Tip)~5A(Max).
所以TPS61175不适合。
HI
建议用外部MOS的升压芯片来做,因为输出72W,输入5V,那么输入的峰值电流都接近20A。
可以考虑用TPS40210, LM3478, LM3481这类芯片来做,因为输出功率非常大,而芯片的驱动力可能不够,需要增加驱动芯片。