This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps562200 5V输入输不出5V

Other Parts Discussed in Thread: TPS562200

datasheet上的输入范围是4.5V~17V,当输入为5V时tps562200输出只有4.2V左右,只有输入电压大于6.5V时才能输出5V,电路和EVM是一样的,请问这是什么原因?