This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: 关于输出电压的问题

Part Number: BQ25756


请教:

 BQ25756是否必须接电池才能正常工作,空载或接纯阻性负载时是否能正常工作?

 现象:

输入12V,设定输出电压值为25.5V(BAT与FB之间的电阻为249k,FB与FBG之间的电阻为16.5k),空载时输出的电压为12V,调整输入端的电压,输出(BAT)与输入电压一致。

相关寄存器的值如下:

REG0x14_Precharge_and_Termination_Control:0xf
REG0x17_Charger_Control :0xc9

REG0x21_Charger_Status_1 :0x2
REG0x22_Charger_Status_2 :0x80
REG0x23_Charger_Status_3 :0x0
REG0x24_Charger_Status_4 :0x0

  • 感谢您对TI产品的关注!
    关于你的咨询, BQ25756是一款具有双向功率流支持的电池充电控制器,主要用于锂离子、锂聚合物或磷酸铁锂电池。
    在空载或接纯阻性负载时,BQ25756可能无法正常工作
    如果没有连接电池,输出电压可能会与输入电压一致,而不是设定的输出电压。因此,为了确保BQ25756的正常工作,建议连接电池。