This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【急求指点!】升压器选择



您好!目前我想找到一款升压器满足下列特征:

我设计了一个太阳能电池阵列,输出电压在3.6V,输出电流在50A, 想找到一款升压器件(或多个器件组合),得到110V的交流电压

目前我想到的选择有二:

1. 将3.6V直流直接转换成110V交流的DC-AC升压器,但目前在市场上只能找到12VDC-110VAC的款式,再低的输入电压很难找到

2. 先将利用DC-DC转换器将3.6V直流转换成12V直流,在用1转换成交流,但目前也未能找到较好的器件。

我对此领域了解不多,恳请专业人员帮我分析上述两种办法是否可行,或者有无更好建议。

  • 亲;是3.6V50A吗?貌似叠砌有问题,线损不知咋样。

    对于这种等级,建议用开环推挽+变压器升压到你期望的DC160V或DC330V,然后直接逆变即可。