This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1117IDCY应用问题:根据公式选择的电阻进行输出电压设置,实际输出不是5V。为什么?



使用TLV1117IDCY将12V变为5V,电流需求是0.5A。电路图如下所示,输出不是5V,而是6.3V,为什么?

为了输出正确电压,只能调整两个电阻R1=6.8K,R2=13.2K时,输出5.3V,为什么?这与公式完全不匹配啊。