This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3488调试中碰到问题

Other Parts Discussed in Thread: LM3488

我们用LM488做的boost电路,输入为12-36V宽压输入,输出为36V,电流为1A;调试中发现在输入用大于24V输入时,输出的纹波电压大概为1.5VPP,而输入电压逐渐变小纹波电压也逐渐变小,在输入电压为20v时,纹波电压几乎消失;

问题1:用输入电压大于24V输入时发现,LM3488芯片控制下MOS管G极的开关信号,为断续工作模式,工作一段时间,停止一段时间,周期大概2ms左右,这种情况是否正常;

问题2:如果在FB分压电阻中与vout连接的电阻上并联一个15nf的电容,输出中纹波电压基本也会消失,但是LM3488芯片控制的MOS开关信号好像也是断续工作模式,这个情况正常么?