This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40200为什么GDRV脚一直输出一个与供电电压相等的高电平?



RC脚输出的是一个正确的锯齿波,SS脚输出的是一个397mV的电压,COMP脚输出的是一个2.4mV的电压,FB脚的电压为75.2mV,ISNS电压也与供电电压相等为22V,反馈电阻我接的是51K和8.3K,想得到一个输出为5V的电压。以上所测得的值都是在接好拓扑线路后测得。当去掉拓扑后只给芯片供电的情况下,测得FB脚的电压为0.9V多,而不是基准电压0.7V。芯片可不可能已烧掉。