目前写1寄存器2b能对外放电(boost),写1b能对电池充电(buck),除非同时插入充电和放电,否则,两种状态,总有一个本能检测到,求解
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前写1寄存器2b能对外放电(boost),写1b能对电池充电(buck),除非同时插入充电和放电,否则,两种状态,总有一个本能检测到,求解
如果在buck充电时,PMID也会有5V左右输出(如果输入源是5V的情况下),不过这个5V是Vbus的5V经过一个防倒灌器件后直接给到PMID的,不是boost升压得到的。
以上谢谢!
谢谢了,目前还卡在这里,当VBUS接5V时,此时要给电池充电,充电状态怎么判断?(1寄存器设为2B默认对外放电状态,同时,PMID给外部放电(接负载),此时读8寄存器,只有在VBUS接5V能读到放电状态,如果PMID不给外部放电(接负载),只在VBUS接5V,读不到放电状态,这是什么情况,有什么好的方法没)
请问下,插入适配器时,PMID测试也有5V左右,这个可以带负载吗?目前我们设计要求插入适配器时,PMID不要对外充电。PMID用于对外充电。另外PMID能不能检测电流的功能实现空载检测?