This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210 boost电路一些问题,大问题!加什么电压,就什么电压输出、、

Other Parts Discussed in Thread: TPS40210

 这两天做了一个TPS40210的升压电路,想从12V升到24V,Io=2A。电路参照datasheet的第一个应用电路,参数就输出电容从40uF换成了100uF,栅极驱动电阻从3.3Ω改成了10Ω。

 

在Layout方面也参考了该芯片的评估板,考虑了单点接地,

可是上电后输出为电源电压,电路直通了,MOS管根本没工作。MOS用的TI的CSD17505贴片MOS,开启电压1.5V,是一片低压MOS,TPS40210的GDRV输出电压为7V, 电流400mA。之前做过这个电路来驱动IRF540N,但也驱动不了,后来才换成了CSD17505但还是工作不了。

  用示波器观察GDRV没有输出,1脚RC振荡波形正常,为350KHz左右。

频率与计算参数差不多,2脚电压为900多mV,没有重启充电的现象,3脚悬空,4脚COMP端输出一个190mV左右的直流电压,这里居然不是锯齿波。5脚FB端有时测得190mV左右,有时又为450mV左右。但是按照输出电源电压12V,通过分压比计算应该为450mV,电流反馈端没信号,因为MOS压根没工作。9脚VBP端输出8V左右。整个电路处于异常状态,芯片也没自动重启。

  后来重新上电测试,听到MOS管在叫,测了一下栅极波形

这是占空比为3.5%的一个尖峰脉冲,电压也不是正常的驱动电压8V ,但这时测得2脚SS端电压为2V左右,FB端450mV左右,但还是没有正常工作。

   请大神们帮帮忙,这个板子我花了三天时间,做了5块测试板,改了各种参数,布局都出不来结果,网上有人用这个芯片大多是带不动负载,我这个连电压都升不上去,都快奔溃了,跪求大神帮忙~@-@