This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295的I2C电平状态及上拉电阻问题

Other Parts Discussed in Thread: BQ24295

请问TI的工程师:

1.BQ24295的I2C SCL,SDA以及 INT信号 三个引脚能否通过上拉电阻上拉到 Vsys来使用?

若可以,那么当Vsys为0V时(Q4断开),SCL,SDA,INT 全变为低电平,此时BQ24595能否正常工作?

SCL,SDA全是低电平是否会使BQ24295进入错误的状态?(datasheet中说空闲时I2C的信号需要为高电平。)

2.若SCL,SDA上拉到Vsys且Q4断开时,当插入充电器后,SCL,SDA两个信号同时变高,是否会对BQ24295产生影响?

3.我的系统中,由Vsys通过外面串接一个MOSFET来给MCU供电,SCL,SDA,INT信号直接上拉到MCU电源。MOSFET由单独的一个小单片机控制。

设备关机时,断开MOSFET来彻底断开MCU供电,以达到省电目的。这时SCL,SDA,INT三个信号全部变成低,

能否采用这种方式使用BQ24295?此时,SCL,SDA,INT信号的漏电流大概多大?(即直接将SCL,SDA,INT接到0V时的电流,

在手册未找到这个参数。)