TPS555355,输出Imax=30A,据说在12V输入,1.5V输出时可以达到最高效率 90%,也就是实际输出电流可达到27A
现在我有一个芯片,满载时电流需求为26A,我这里是5V输入,1.2V或者1.8V输出,,电流26A
在电源芯片选型时,一般普通的电源芯片需有20%的余量,也就是,普通的电源转换芯片,我需要选择大于等于32.5A最大电流输出的芯片才可以正常供给26A的实际需求
可以想象,TPS555355最高效率时为27A输出,感觉有些冒险。不知道是否可以使用?
市面上超过30A输出的稳压芯片相对较少,TI好像有几款40A输出的,我是否有需要选择40A的保险些呢,或者大家是否有别的芯片推荐给我,谢谢各位了!