This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教LM3404HV buck降压电路的问题

Other Parts Discussed in Thread: LM3404HV

我采用LM3404HV来DC-DC降压,我是输入55V,800mA左右,输出29V,700mA,即要求输出20W。

但我的电路开始有输出,但是只有6V多左右,检查发现DIM引脚接地了,将DIM引脚悬空后,测得芯片的1脚和5脚间还是6.5V,输出也是6,5v;后来就芯片烧掉了,请专家帮着分析下我的图。谢谢了!

新建 WinRAR ZIP 压缩文件.zip