This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65130 正负电压DCDC 负输出不正常

Other Parts Discussed in Thread: ISO124, TPS65130

1  : TPS65130状态: +5v输入,正负15v输出,原理图是按照手册上的电路进行设计的,正负15v供给6个隔离运放ISO124供电。TPS65130手册上图3有说明,在正负15v输出下电流应该在100mA左右.  而ISO124连续工作电流要求15mA,6个也就是在90mA左右,基本满足要求。


2:实测值: VREF =1.21v(正常值为1.213v,正常),VFBP=1.2v(正常值为1.213v,正常),VFBN=1.11v(正常值为0v,不正常),输出VPOS=14.85(正常),VNEG=0.25V(正常值为0v,不正常)。初步来看应该是由于VFBN这个参考电压不为0导致的输出NEG不正常。


3:检查措施:仔细检查了电路板,暂未发现漏焊错焊韩反的现象。本人有一个不确定的地方是:INP INN OUTN这个 器件收都是2路,而我这个设计只有了一路,另一路是悬空的,不知道有没有问题。另外仔细检查发现我接的INP是第1脚, INN是第5脚,而OUTN是第14脚,如果单路可以工作的话,我是不是应该接第13脚的OUTN。


4:附件是原理图,请查阅。


5:其他问题暂时没有发现,请赐教。

tps65130.docx