This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助! 电源方案选型(控制芯片)

Other Parts Discussed in Thread: UCC28740

交流输入:90~264   Vac

输       出:12V / 2A

输入频率:47~63     Hz

输入电流:0.8           Arms            Max

浪涌电流:80            Arms            Max

效率:       86%                             Min

空载功耗:75            mW              Max

泄漏电流:  100           uA                Max

有电路保护功能

拓扑的话,我选择Flyback,希望大家提建议,多谢!