This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650243的DCDC3的问题

Other Parts Discussed in Thread: TPS650243

各位工程师好,最近在用TPS650243这个PMIC,输入是USB的5V(范围大约4.5~5.5V吧),需要输出3.3、1.8和1.2V(都是DCDC),原理图见附件。

设计的上电顺序是DCDC3的1.2V先输出,这个1.2V上升超过1V的时候nPWRFAIL脚会释放,进而nPWRFAIL信号会变高,使能1.8V和3.3V的输出。

然而上电之后却发现1.2V的空载输出只有大约700~800mV,这时芯片的输入电流很小,芯片也没有异常发热;如果将一路LDO的输出(1.2V)接到DCDC3的输出上,那么其他两路DCDC在被使能之后可以正常工作。

贴了三套都是这个现象,应该不是焊接问题,电感和其他元器件的选型应该也没有问题,布局也很简单。

还请各位工程师帮忙分析一下可能的原因,谢谢!