Other Parts Discussed in Thread: TPS74901, TPS54519, TPS54427, TPS54528
如题,为了减小热量损耗和降低功耗,需要得到0.9V,满负载4A电流,工作温度小于等于70度,请问有什么方案推荐呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LDO的目的是将纹波降到最低,DCDC纹波对于高速通信总是有点大。目前的方案是DCDC+两级LDO,发现LDO的电流最大只有4A,而且是常温下,使用过程中发现电流大了以后输出电压就降低太多,能否有更高驱动能力的0.9V的LDO呢?
目前用的是TPS74901,两级LDO降压到0.9V,才发现是3A的,还没有到4A,导致压降在电流超过3A的情况下降低了,请问有没有4A以上能降到0.9V的LDO呢?或者能否采用两个74901并联呢?
Hi
采用DC/DC的芯片,然后在增加以及LC 也可以将纹波做得非常小。
大电流不建议选择LDO,功耗太大,而且LDO不能被并联,因为他们不能均流。
多谢回复,好想加入你们TI,不过没有机会。
我已经选用了凌力尔特的LT3071了,能到5A,0.9V的LDO。
Hi
不客气,请问你的输入电压是多少伏? 用LDO,温度控制在70℃, 除非你的输入电压也很低。
LDO的前一级是DCDC,之前采用的是TPS54427,觉得都要做到5A,就改用了TPS54528。为了达到最小的纹波和最小的LDO热耗散,DCDC输出设置为1.2V。