This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: 技术咨询

Part Number: BQ27Z746


你好,

      在电路设计中使用BQ27Z746(原理图如下),有以下几个问题需要帮忙确认一下,谢谢!

1、电路需要有“0V”禁充功能,电路中R12需要多大阻值?当前电路合适吗?

2、电路中支持精密电阻是1~20毫欧,当前已用电路采用是2毫欧的精密电阻,实际电路工作充电是200mA, 放在在1mA以内,请问:电量计参数有如下几项如何设置比较符合实际要求?

3、如上电路需要过UL认证,增加一个二保电路(U2), 与电量计搭配有双保护电路,请协助评估此电路是否有什么缺陷或隐患?

4、电量计在烧录过程中偶发出现断电,导致板子无法激活或者进入了ROM模式,有什么方法来恢复正常(板子有通讯且能够激活)?