This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700-Q1: UCC28700-Q1输出电压异常(请帮忙分析一下具体原因)

Part Number: UCC28700-Q1


您好!

        我们目前在使用TI的电源芯片UCC28700-Q1,设计初始需求是:输入60-500Vdc,输出18V9V两路。目前调试过程中发现一个问题,请帮忙分析下可能是什么原因:

        设计参数:输入电压:60-500Vdc,输出:18V 10W max9V 3W max,辅助绕组15V,变压器匝比:原边:辅助绕组:18V输出:9V输出 = 27784,原边感量:220uH,反馈电阻值:Rs1=70.6KohmsRs2=23.2Kohms,电流采样电阻:0.51ohms,其他部分设计均参考贵司的规格书和参考计算文档。

        目前出现的问题表现是:输出空载,输入60V时,mos管门极只有规格书上启动时的3个波,然后就不再发波,直到此时CS脚最大约250mV,和规格书匹配,但是在mosoff时,VS脚电压仅225mV左右,严重和规格书的4.05V不匹配。怀疑控制IC就此进入报错模式,负载输出电压处无输出。

        具体这3个波时的图片见下图,其中,CH1=输入电压,CH2=VDDCH3=28700 VS脚,CH4=28700 CS脚,CH6=MOS-GS

        IC6个故障模式,此时无输出,所以无输出过压;输入电压确定高于欠压点,负载空载无过温,CS脚无过流和过阈值现象,VS脚电压远远低于4.05V

        因该项目时间节点较为紧急,还请帮忙分析下是啥原因,多谢!