This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3886电流采样不使用current sense amplifier而使用电流霍尔传感器的处理方法



您好,我在设计Boost电路时,由于输出电流平均值是60A,短路电流设定为120A,按照UC3886手册中的方法,最后计算的电流采样电阻值是0.00068-0.0016欧姆,电阻功率是9.812W-23.04W,这样导致采样电阻不好选取,我决定使用电流霍尔传感器,不知道对于current sense amplifier的处理有没有什么要特别注意的。

我的Boost输入电压是23V,输出电压45V,输出纹波电压0.5V,开关频率200kHz,输出电流平均值60A,最大值90A,短路电流设定为120A

  • 亲;对于霍尔,主要是带宽问题。如你所述,200k(1dB)的足以。其余的;如而定环境温度范围、可靠等级、供电方式及零点电压等都是需要注意的,按你的实际应用选择即可。