This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于太阳能MPPT管理芯片SM72442的几点疑问?



最近要做一款光伏组件监控器,需要实现组件电压、电流、温度监测,电弧检测,以及紧急情况下快速关断输出等功能。

查看资料TI的SM3320系列可以实现上述功能以及MPPT功能,我看过应用手册AN2122和AN2124,对于内容有几个问题想咨询一下:

1、功率优化器集成了MPPT功能,输入电压(即光伏板输出电压)是随MPPT进行调节,那优化器输出电压是如何确定的?是由优化器确定还是由外部直流母线电压确定?
2、优化器进入PM模式有两种情况,第一种情况是输入电压和输出电压相差在±2%以内;第二种情况是检测到过温以及过流。我的疑问是过温及过流情况下不应是直接关机吗,怎么会进入PM模式?
3、如果不需要MPPT功能,是否可以只工作在PM模式,在异常情况下仍可以关断组件输出?
 
哪位朋友用过这款是否可以帮忙解答一下,希望能得到TI的FAE工程师指导,谢谢!