This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76905: BQ76905上电后马上SCL和SDA引脚会被拉成低电平

Part Number: BQ76905


  BQ76905上电后会马上将SCL和SDA拉到0电位。但是REGOUT却有3.3V输出。

另外一个现象是,当我MCU给TS脚输一个1.5V的唤醒电平时,SCL和SDA就会变成高电平。

并且我TS上加多长时间的电压,对应的SCL和SDA就会变高多久。

当我把TS脚上的唤醒电平(1.5V)撤销后,SCL和SDA又会恢复成低电平。

另外说明一下。SCL和SDA加的是10K上拉电阻到3.3V