This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60403: TPS60403输出阻抗的计算

Part Number: TPS60403

dears,

我的客户在使用TPS60403时遇到如下问题,请帮忙解答一下:

如下计算公式中,Rswicth是多大?ESRcflyESRco的典型值是多少?这里面的Cfly,ESRcfly, ESRco对应的测试频率是多少?和具体频率有关系吗?

谢谢!

  • 感谢您对TI产品的关注!
    关于你的咨询,Rswicth是多大?ESRcfly、ESRco的典型值是多少?这里面的Cfly,ESRcfly, ESRco对应的测试频率是多少?和具体频率有关系吗?

    A: 输出阻抗的典型值是12ohm,大约15ohm。所以Rswitch大约为1ohm.但是这个值并不是特别重要。
    the output resistance is specified as typically 12 Ω, at most 15 Ω. This implies that RSWITCH is roughly 1 Ω; however, this value is not important.
    EsrCfly和EsrCo:这些参数通常与电容器的等效串联电阻(ESR)有关。对于最佳性能,建议使用低ESR的电容器X5R or X7R types,例如陶瓷电容。
    TPS60403的工作频率为250kHz,因此这些参数通常在该频率下进行测试。

    对于你咨询的这个公式Ro,其实没什么太大的用处。
    只有当您想通过降低C(fly)来减少输出波纹,并且能够承受更大的阻抗时,该公式才有用。