hi,
I have a question for IBAT over current protection fof BQ25620.
When the IBAT over BATFET_OCP 6A, it will be enter HICCUP mode.
how can I recover if we have no external power source.
Does it need to lower IBAT current under 6A?
or does it must be plugged in external power source only?
another question.
If VIN(USB or adaptor) is not plug in ,
and the voltage of VSYS is higher than BAT pin,
Will it have current flowing into the battery through the POWER PATH?
Thanks.
Dylan.