我之前用LM234输出7mA,现在需要增加一倍到14mA,技术手册上写“Programmable From 1μA to 10mA”,意思最大可以输出10mA吗?但是我试过调整电阻值,可以输出14mA,我怕长期工作不稳定,所以请问:需要用两个LM234输出7mA并联吗,还是用一个输出14mA就行?谢谢了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我之前用LM234输出7mA,现在需要增加一倍到14mA,技术手册上写“Programmable From 1μA to 10mA”,意思最大可以输出10mA吗?但是我试过调整电阻值,可以输出14mA,我怕长期工作不稳定,所以请问:需要用两个LM234输出7mA并联吗,还是用一个输出14mA就行?谢谢了。
Hi
如你所说10mA就是最大电流极限,不建议超过10mA的应用。
datasheet: http://www.ti.com.cn/cn/lit/ds/symlink/lm234.pdf 第十一页的高电流输出,你可以参考