之前有做过一款2500*4的计量, 计量出来的值是准确的, 约9K5左右而且充放电百分比曲线也正常,
现在需要做一款2500*8的, 学习步骤也跟上次的类似,dataflash也做调整, 但是为什么学习后, 总容量只有16K? (电芯实际有20K)
而且在放电时. 100%-10%的区间是直线, 但是在10%时会跳到20%,然后继续慢慢下降到10%,重复3次后才会跳到0%
请问有啥可能会导致这种情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前有做过一款2500*4的计量, 计量出来的值是准确的, 约9K5左右而且充放电百分比曲线也正常,
现在需要做一款2500*8的, 学习步骤也跟上次的类似,dataflash也做调整, 但是为什么学习后, 总容量只有16K? (电芯实际有20K)
而且在放电时. 100%-10%的区间是直线, 但是在10%时会跳到20%,然后继续慢慢下降到10%,重复3次后才会跳到0%
请问有啥可能会导致这种情况?
但是我看BQ27542的最大容量也是14AH, 而27541的规格书最大容量标明是32AH??
看样子27542是27541的cost down版本吗?
下面是27541的DS
1FEATURES
23• BatteryFuelGaugefor1-Series(1sXp) Li-Ion
Applicationsupto 32Ahrcapacity
• MicrocontrollerPeripheralProvides:
– AccurateBatteryFuelGaugingsupportsup
to 32Ahr
– Internal orExternalTemperatureSensorfor
BatteryTemperatureReporting
– SHA-1/HMACAuthentication
– LifetimeDataLogging
下面是27542的DS
# Series Cells
Cell Chemistry
Battery Capacity (Max) (mAh)
Communication Interface
Implementation
Gas Gauge Algorithm
Special Features
Operating Temperature Range (C)
Pin/Package
Approx. Price (US$)
BQ27542-G1
Single Cell
Li-Ion/Li-Polymer
14500
HDQ
I2C
Pack
Impedance Track
SHA-1 Authentication
Turbo Mode
-40 to 85
12SON
1.25 | 1ku
在官网上没看到有change list, 下载pdf里面也没有,这是新型号的ic , 只有初始的版本
| 日期 | 修订版本 | 注释 |
|---|---|---|
| 2015 年 4 月 | * | 最初发布版本 |
Copyright© 2015, Texas Instruments Incorporated. An IMPORTANT NOTICE at the end of this data sheet addresses availability, warranty, changes, use in safety-critical applications, intellectual property matters and other important disclaimers.
手册上 6.1.1.7 ,
For battery capacities larger than 6 Ahr, Design Energy Scale = 10
is recommended.
把 Design Energy Scale 改为 10 , 是否可以解决容量 20Ah 的问题?