Other Parts Discussed in Thread: TPS92510
图二是我的tps92510恒流电路图(图一是从ti网站上有个电源设计工具而来,我的电路与推荐电路不同之处主要在于输出滤波电感较大,电容也较大),用15V供电,驱动6只LED(理论上当电流0.7A时,led串两端电压为13.5V),预想LED电流为0.7A左右。
上电后,在PWM1处输入3.3V,200HZ,占空比50%的方波,发现亮度微弱,用万用表测得流过LED的电流为0.01A。将占空比从50%增大到95,发现亮度强一些,但仍然微弱,用万用表测得流过LED的电流为0.02A。都没有达到我的预期0.7A左右的效果(led电流无论是0.01A还是0.02A,LED间电压均为9.5V左右,感觉此电路不是恒流源而是恒压源了),请问什么原因?