如上图的升压电路,需要输入5V输出15V。 但在实际连接中,一上电34063就被烧坏,很烫手,在通电钱也检查过了没有发现短路的地方,现在不太清楚为什么会这样子?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电感用的是 :绕线贴片功率电感 101
二极管是:RS1M 快恢复二极管
提供的5V电源是由一块转换板转换过来的(220V-5V)
Hi
最大输出电流是多少?
电感不应该选择10mH这么大,一般200uH左右,重点是饱和电流要足够.