This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: 除了电压还有什么条件触发永久失效的SOV状态?

Part Number: BQ28Z610


您好:

       我用的BQ28Z610,两节串联,完成第二轮学习的时候,电池在放空电状态,两节电压都在3060mV,Update Status=0x14,由于0x14这个值跟芯片资料的值不一直,所以准备重新进行学习,

       于是我们发送0x41复位芯片,发送0x21重新使 Manufacturing Status [GAUGE_EN]=1,这时发现 LStatus[ITEN] 一直等于0,不再跟随 GAUGE_EN 变化,这个时的 Update Status 一直等于0x10,我没注意这时的SOV是否等于1。在没法高清楚原因的情况下,我准备给电池先补一些电,继续进行新的学习。

       当开始充电的时候,发现无法充放电,充电器电压设置8.4V。检查原因发现芯片进入SOV状态,相关设置:Permanent Fail>SOV>Threshold=4330mV,Delay=2S,电芯确定没有过压,是什么条件触发了这个状态?