This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

升压芯片TPS61030问题



工程师: 

          你好,本人想通过锂电池3.6~4.2v输出4.2至4.5v电压控制GPRS工作,要求输出峰值电流2A;有二个问题不是太理解:

        1、这个芯片可以实现我这个功能吗?

        2、如果输入电压大于4.2v,输出电压还是保持4.2v还是随着输入电压的升高而升高呢?

         谢谢!

  • 亲;锂电最低输出电压大约2.3V,你的指标可能需要再商讨一下。

    如果最低3.6V;没有问题,可以出2A。如果2.3V,就不够了。

    亲;这个IC可以4.2V入4.2V出。