Other Parts Discussed in Thread: LM27313
新人学习,使用了LM27313芯片做了个升压电路,空载时电压24V,但是在带载时候输出电压会上升到30V。且输出电压不稳定,求解决办法
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM27313
新人学习,使用了LM27313芯片做了个升压电路,空载时电压24V,但是在带载时候输出电压会上升到30V。且输出电压不稳定,求解决办法
你好,怀疑FB被干扰了,PCB贴一下,反馈回路分压需在芯片端,谢谢。
你好,PCB采用的是双面板,将芯片,电感和二极管,放在一面上。输入电容,输出电容以及反馈回路放在另一面上。如果是被干扰了的话,怎么去解决这个问题呢?在FB端到地接一个电容能改善这个问题吗?新人,第一次使用,还望能解答清楚些,谢谢!
有测量FB,在带载时候为0.12V,推测是FB低了导致输出一直升高,而我选用的二极管是B130LAW,反向击穿为30V,将电压箝位在30V了。
后来测试换了二极管,开机瞬间电压上冲至50V,将LM27313的内置mos管烧穿,SW端与地短路。现在感觉就是FB端电压没有从输出电压正确采样过来,FB端接的是EA的输入端,在加电前是对地短路。加电后FB端对地变为600多欧,芯片已被烧坏。