This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCDC ±12V输出



现在有个项目需要±12V供电,想问问如下方式能实现同一块PCB上的±12V供电吗?

图中DCDC芯片用的是两片LM2576HV-12,C12是电压(MAX:50V DC)输入端,12V负载电流1-1.5A,-12V负载电流400mA。

谢谢!

  • 你好,负电压那路有些问题,开始输入电压50V,当输出电压建立时,输入电压相当于62V,不推荐,最好保证最终输入电压低于60V,谢谢。

  • Hi Frank,

    谢谢你的回答,我还有个疑问请教一下,﹣12V输出相当于是将﹢12V输出的地端做输出,正输出端做地,不知道这个理解对不对。

    而此时+12V的输出地理论上是接到另外一路+12V(用于输出-12V的那一路)的正输出端的,这个+12V输出会受影响吗?

    表达混乱,不知能否看得懂哈,汗、、、

    谢谢!