TI的技术支持:
你好!需要推荐一款电源芯片,输入、输出参数如下所示:
输入电压:6.5V~8V(电池电压);
输出电压:7.2V(正负10%);
输出电流:3.1A(最大值)
在WEBENCH上仿真得到一款芯片LM5157,但这款芯片价格较高、体积也太大,希望专家可以给推荐一款价格便宜、体积小的芯片,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.