TPS63031 datasheet上关于Power Saving模式,有这么一句话:“Connecting a clock signal at PS/SYNC forces the device to synchronize to the connected clock frequency。” 感觉 PS/SYNC需要接一个时钟周期信号?能不能只接一个普通的高低电平,直接用MCU的普通I/O高低电平控制,而不是一个时钟信号?
另外,使用使用Power Saving模式后效果怎么样?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
见参数表: Frequency range for synchronization: 1250 ~1800 kHz
所有占空比在50%左右的方波信号都应该是可以的,例如时钟芯片,或者带时钟功能的芯片
Hi
Powersaving模式主要是用于提高芯片的轻载效率,见datasheet: http://www.ti.com.cn/cn/lit/ds/symlink/tps62260.pdf 第十四页
可以比较图7/8或者9/10,1mA负载时powersaving模式在效率90%左右,但是PWM模式下只有20%左右。
多谢 Johnsin Tao的回复。我不太明白的是为什么需要加一个同步时钟,TPS63031是多相电源吗?加在PS/SYNC的这个同步时钟作用是什么?
在我们设计的场景中,DC-DC的负载会有相当长的时间处于休眠状态。这个时候只需要很小的负载电流。这个时候,我能不能直接把PS/SYNC信号拉低,让TPS63031处于Power Saving模式,待设备解除休眠前,再拉高PS/SYNC信号? 这样做是否能达到降低功耗的效果?
再次感谢Jonhsin Tao周末晚上加班回复
TPS62260的datasheet确实比TPS63031的datasheet要详细一些。在仔细参考TPS62260datasheet前,烦请Tao帮忙澄清一下两个概念:
1)PFM模式是否就是指单纯拉低PS/SYNC管脚?当处于PFM模式,如果输出电流减小到一定阈值,自动进入Power Saving。
2)PWM模式就是指在PS/SYNC管脚接某个频率的PWM同步信号?